U-Boot powerpc MPC8309 TEXT_BASE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-Boot powerpc MPC8309 TEXT_BASE

1,902件の閲覧回数
ganjiaravind
Contributor I

Hi, everyone here i have a question in u-boot source code ,when u-boot.bin is loaded from NOR Flash we consider the TEXT_BASE value as 0XFFF0_0000 in case of (RCWHR[BMS] is 1) and this address will match with the flash device address over Local Bus ,But when u-boot.bin need to get from an SD-card or a SPI EEPROM device what will be the TEXT_BASE and how we relate that value to the address over booting device (SD/MMC,SPI) ,can anyone here to help me in understanding

                       thanks in advance.

0 件の賞賛
返信
1 返信

1,593件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Booting from SPI or SD-card is performed with using onchip ROM, in this case the core starts from this onchip ROM, performs some initialization (SPI or SD-card driver bring up), and then loads firmware from specially formatted SPI or SD-card, and than run it. Because of this reason, special "ramboot" version of U-boot should be used. For more detailed description please please look application note AN3659. This document is not directly applicable to MPC8309, but can be used for better understanding

https://www.nxp.com/docs/en/application-note/AN3659.pdf 

Regarding your question about TEXT_BASE - for MPC8309 this parameter should be 0x01000000


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信