TWR-MPC8309 local bus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TWR-MPC8309 local bus

1,078 次查看
bbutler
Contributor I

I am trying to determine if I can use the TWR-MPC8309 local bus to connect to a TWR-LCD module and to my custom peripherals. Looking at the schematic, they don't make sense to me:

- Data bits 0-7 seem to be reversed. MPC_LBC_D0 is hooked to bus D7, MPC_LBC_D7 is connected to bus D0, etc.

- Address bits are likely strange MPC address bits 25 downto 6 are connected to bus address bits 0 to 19. The address bit numbers don't even match.

- Shouldn't the signals on the backplane be connected to the multiplexed bus (the MPC_LBC_LAD* signals) instead of the demultiplexed signals?

Am I just missing something? I'm not seeing much documentation on the MPC8309 module, so I'm having to make a lot of guesses based on what I'm seeing in the schematics.

标记 (3)
0 项奖励
回复
1 回复

967 次查看
lunminliang
NXP Employee
NXP Employee
0 项奖励
回复