T4240 thermal diode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T4240 thermal diode

1,720件の閲覧回数
jeffcao
Contributor I

I find the T4240 has have two on-die diodes,but I cant find Their differences.

in datasheet only introduce which pin is thermal diodes

I want to know which issue I need use two diode

and which issue i only use one diode 

thank you

0 件の賞賛
返信
1 返信

1,484件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

There are two thermal diodes located at different locations on the die. One that is close to core clusters and the other one is more close to platform logic, thus each diodes has two pins the cathode and the anode, you need to use the cathode and anode to measure temperature for each site/diode. Some times there are difference in temperature between different sites on die, the difference can be large, up to 20C in extreme cases and thus it is wise to do measurement on both available sites.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信