T1042 processor JTAG ISSUE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1042 processor JTAG ISSUE

4,170 Views
utkarsh
Contributor I

Hi All 

We have T1042 processor , currently we have populated the resistor ,capacitor and IC related to only power supply & JTAG . We are able to power it on but when on connecting  JTAG with code warrior we are facing issue 

Jtag leds are ok but configuration are not ok . Moment we are running code program with code warrior .We get the error 

Error launching t1042-core 00_SRAM _T1042_Connect 

CCSProtocolPlugin: Failed to correctly configure the JTAG chain  

 

On hardware level we have checked 

1. Power supply working 

2. jtag reset is working

3. Jtag connection are varified 

Kindly provide the answer for the same . 

 

Thanks 

 

 

 

0 Kudos
Reply
6 Replies

4,039 Views
utkarsh
Contributor I

Hi

Based on hardware design against AN4825  changes are made but still no success. . 

Please find the attached RCW.txt file 

Hardcoded RCW is 0x9E wrt RCW value are changed (only jtag configuration settings changed) 

We are trying to detect processor in the JTAG chain 

Also attached the scanboard command screenshot, not able to detected processor IDcode . 

 

0 Kudos
Reply

4,020 Views
utkarsh
Contributor I

Hi 

More to  add on 

On our processor we have mounted only power supply related components (IC, resistor ,etc) which is working. 

JTAG related components also mounted on the hardware (Hardcoded RCW is 0x9E)

Now when we are running code warrior projects through SRAM (since DDR is not mounted on Hardware), we are getting Pop up ERROR " FAILED to configure JTAG chain " 

 RCW file have attached in my earlier post & made changes for JTAG. i.e. 0x9E

Is it ok to keep the RCW default values for other peripherals since on the board other than JTAG there is nothing else mounted.  

 

 

 

0 Kudos
Reply

3,993 Views
khushbur
NXP TechSupport
NXP TechSupport

Hi @utkarsh 

 

Can you please provide your schematic here for further debugging. If not please create new technical case using below link.

https://support.nxp.com/s/

I would also recommend you that in order to follow this request,
please do not forget to mention on the case description this case number
which is: # 00566644

 

Thanks

Khsuhbu

0 Kudos
Reply

4,103 Views
khushbur
NXP TechSupport
NXP TechSupport

Hi @utkarsh 

 

It seems that there is no valid RCW on the target board.

Please refer to "Table 4-12. Hard-Coded RCW Options" in T1042 Reference Manual to configure the your custom board as hard-coded RCW.

 

Thanks

Khsuhbu

0 Kudos
Reply

4,100 Views
utkarsh
Contributor I

Hi Khusbur 

Further investigation, I found something weird.

On giving CCS command

source IPCODE.tcl  or scanboard

It did not received the JTAG IDCode .Looks like processor itself didn't recognized.  

Does it still required RCW configuration,since the processor itself not recognized. 

Where all areas I can look ?? 

Kindly suggest 

 

 

 

 

0 Kudos
Reply

4,056 Views
khushbur
NXP TechSupport
NXP TechSupport

Hi @utkarsh 

 

Does it still required RCW configuration,since the processor itself not recognized. 

Yes. 

Where all areas I can look ?? 

Please verify your hardware design against AN4825

 

Thanks

Khsuhbu

0 Kudos
Reply