T1024 - core clock frequency speed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

T1024 - core clock frequency speed

跳至解决方案
2,496 次查看
giacomo_gaspari
Contributor II

Hi,

due to chip shortage we'll have to evaluate T1024NSE7PQA (F_core_clk=1400MHz) instead of actual T1024NSE7KQA (F_core_clk=1000MHz).

From the manual it seems that using the alternative chip would be possible without changing any RCW or other FW/HW data.

Could you please confirm my hypothesis?

标签 (1)
0 项奖励
回复
1 解答
2,491 次查看
ufedor
NXP Employee
NXP Employee

Your understanding is fully correct.

The 1400 MHz part can be used in place of the 1000 MHz part without any change in hardware and firmware.

在原帖中查看解决方案

1 回复
2,492 次查看
ufedor
NXP Employee
NXP Employee

Your understanding is fully correct.

The 1400 MHz part can be used in place of the 1000 MHz part without any change in hardware and firmware.