@ufedor Sorry for late reply, due to current pandemic situation we were not able to work on the same.
Please check whether the IFC_CSORn_GPCM[PTO] is small, so timeout during ASIC read is possible.
We have tried both minimum value and maximum value of IFC_CSORn_GPCM[PTO] , still we are facing the same issue. Although on increasing the GPCM[PTO] the frequency of such instances decreases sharply.
Refer to the e5500 Core Reference Manual, 4.9.3.1 General Machine Check, Error Report, and NMI Mechanism.
We have referred to the recommended manual and we found that MCSR[a000] refers to LD and LDG bit.
We are still not able to find the root cause of the problem . Refer to the attached image for description of LD and LDG bits.
We have one more query regarding the above issue , when we are floating the cycle on the state machine of the ASIC device, then there is probability that the processor and ASIC device are driving at the same time leading to contention. What will happen in this case due to contention, will it cause MCSR issue or this will switch off the processor device?