T1022: Serial8250: too much work for irq37

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1022: Serial8250: too much work for irq37

ソリューションへジャンプ
1,769件の閲覧回数
hemwant
Contributor IV

I am having a T1022 processor based board, the uboot is booting from spi and nand flash is used to boot kernel, device tree and file system. When i am booting kernel  it sometimes got struck in kernel giving error too much work on irq37. This behavior is very frequent . Please look into the attached kernel log for reference.

Processor : T1022

Reset Configuration Word (RCW):
00000000: 0c10000e 0e000000 00000000 00000000
00000010: 85000000 00400112 ec110000 21000000
00000020: 00000000 00000000 60000000 0003a000
00000030: 00000000 d416aa05 00000000 00000000

タグ(1)
0 件の賞賛
1 解決策
1,595件の閲覧回数
hemwant
Contributor IV

In our case there was a device[ATMega128] connected to one of processor UART, we were sending some UART data to the device on linux boot up. On commenting the same the issue did not occur again. To completely solve the problem we programmed our atmega128 device. Thereafter the issue didn't occur.

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
1,761件の閲覧回数
ufedor
NXP Employee
NXP Employee

It looks like UART hardware generates break condition - check UART SIN signal level.

0 件の賞賛
1,596件の閲覧回数
hemwant
Contributor IV

In our case there was a device[ATMega128] connected to one of processor UART, we were sending some UART data to the device on linux boot up. On commenting the same the issue did not occur again. To completely solve the problem we programmed our atmega128 device. Thereafter the issue didn't occur.

0 件の賞賛