Segger J-Link with LS1046A Freeway

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Segger J-Link with LS1046A Freeway

ソリューションへジャンプ
2,899件の閲覧回数
jekim
Contributor IV

Hello,

I installed CodeWarrior Studio 11.5.2. I'm trying to add new connection for LS1046A Freeway. It seems the probe type is fixed to CWTAP. Is it possible to add segger J-Link in the connection? Thanks.

Best Regards,

Jeff

タグ(3)
0 件の賞賛
返信
1 解決策
2,895件の閲覧回数
ufedor
NXP Employee
NXP Employee

You wrote:

> Is it possible to add segger J-Link in the connection?

This is not possible.

元の投稿で解決策を見る

3 返答(返信)
2,896件の閲覧回数
ufedor
NXP Employee
NXP Employee

You wrote:

> Is it possible to add segger J-Link in the connection?

This is not possible.

2,885件の閲覧回数
jekim
Contributor IV

Dear Fedor,

 

Thank you for the confirmation. Then, below base unit and tip are enough for LS1046A Freeway debug?

CWH-CTP-CTX10-YE Product Information|NXP

CWH-CTP-BASE-HE Product Information|NXP

 

Best Regards,

Jeff

0 件の賞賛
返信
2,878件の閲覧回数
ufedor
NXP Employee
NXP Employee

Yes, these are correct TAP and Probe Tip for ARM processors.

0 件の賞賛
返信