Running Automatic Applications

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Running Automatic Applications

1,143 Views
narreddisivapra
Contributor II

Hello,

             I am using MPC8323E-RDB board for Linux application development. I want to run my C application automatically right after boot-up. How can I achieve this on my board. Please, respond as soon as possible.
Thanks and Regards,
Siva Prakash Reddy N
Tags (1)
0 Kudos
Reply
3 Replies

1,018 Views
Pavel
NXP Employee
NXP Employee

It is common question for Linux.

See the following pages:

http://unix.stackexchange.com/questions/56957/how-to-start-an-application-automatically-on-boot

 

https://docs.oseems.com/general/operatingsystem/linux/automatically-run-program-on-startup

 

http://stackoverflow.com/questions/7221757/run-automatically-program-on-startup-under-linux-ubuntu

 

http://superuser.com/questions/685471/how-can-i-run-a-command-after-boot

 

http://www.linuxquestions.org/questions/linux-general-1/how-do-i-automatically-start-a-program-at-st...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,018 Views
narreddisivapra
Contributor II

Thank You for your help.

Now I wanted to remove terminal from my MPC8323E-RDB board i.e, it should not appear after boot-up, so what can I do to knockoff terminal.?

Please, Reply as soon as possible.

Thanks and Regards,

Siva Prakash Reddy N

0 Kudos
Reply

1,018 Views
narreddisivapra
Contributor II

Hello,

          Please respond to my query as soon as possible.

Thanks and Regards,

Siva Prakash Reddy N

0 Kudos
Reply