Rev1.1 finished good part number will have an 'A' suffix and the mask on the packaged part will read 1M17Y.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Rev1.1 finished good part number will have an 'A' suffix and the mask on the packaged part will read 1M17Y.

跳至解决方案
1,424 次查看
troy_mcclellan
Contributor I

How do I determine which die revision MPC8308 that I have installed in my products.

Which register in the CPU can I remotely read?

0 项奖励
回复
1 解答
1,303 次查看
alexander_yakov
NXP Employee
NXP Employee

The difference between silicon revisions 1.0 and 1.1 may be determined by reading "System Version Register" (SVR)

Rev 1.0:  SVR = 0x8101_0110

Rev 1.1:  SVR = 0x8101_0111

This information is specified in MPC8308 Reference Manual, Table 7-1.

For the functional difference between silicon revisions 1.0 and 1.1 please look MPC8308 Device Errata.

Here is a direct link to MPC8308 documentation page:

Low-Power PowerQUICC II Pro Processor with DD|NXP


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,304 次查看
alexander_yakov
NXP Employee
NXP Employee

The difference between silicon revisions 1.0 and 1.1 may be determined by reading "System Version Register" (SVR)

Rev 1.0:  SVR = 0x8101_0110

Rev 1.1:  SVR = 0x8101_0111

This information is specified in MPC8308 Reference Manual, Table 7-1.

For the functional difference between silicon revisions 1.0 and 1.1 please look MPC8308 Device Errata.

Here is a direct link to MPC8308 documentation page:

Low-Power PowerQUICC II Pro Processor with DD|NXP


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复