Reset vector of 8641

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reset vector of 8641

3,036 Views
ravindrakulkarn
Contributor II

The reset vector of 8641 is mentioned as 0xFFFF0100 in the data sheet (section 2.2.6 of MPC8641DRM.pdf)

it says

the e600 cores fetch their reset vectors by performing

a burst read from effective address 0x0_FFF0_0100 and begin executing with the instruction at effective

address 0x0_FFF0_0100.

However the u-boot-2010.09 code assumes the  reset vector at 0xefff0100

See the extract of u-boot.map below.

Please explain this discrepancy in the reset vector.

Note: The HPCN board, uses default boot configuration (does not use i2c boot eeprom).

.text           0xeff00000    0x48e24

  arch/powerpc/cpu/mpc86xx/

start.o(.text)
.text          0xeff00000     0x2714 arch/powerpc/cpu/mpc86xx/start.o
                0xeff0011c                _start_of_vectors
                0xeff02648                setup_ccsrbar
                 0xeff00004                version_string
                0xeff02408                relocate_code
                0xeff023f8                in32
                0xeff02100                early_bats
                 0xeff023f0                in16r
                0xeff026c0                unlock_ram_in_cache
                0xeff023b8                in8
                0xeff02400                in32r
                0xeff023c8                out16
                 0xeff0262c                enable_ext_addr
                0xeff023e8                in16
                0xeff02208                disable_addr_trans
                0xeff02228                transfer_to_handler
                0xeff00100                _start
                0xeff023a4                dc_read
                0xeff023d8                out32
                0xeff023a8                get_pvr
                 0xeff023d0                out16r
                0xeff020ac                invalidate_bats
                0xeff023c0                out8
                0xeff01fa4                _end_of_vectors
                 0xeff023e0                out32r
                0xeff02578                trap_init
                0xeff00110                _start_warm
                0xeff021e4                clear_tlbs
                0xeff023b0                get_svr
  arch/powerpc/cpu/mpc86xx/traps.o(.text)


6 Replies

2,464 Views
scottwood
NXP Employee
NXP Employee

The address that U-Boot is linked at is the address it will be running C code at, prior to relocation to RAM.  It is not the actual address that the first instructions execute at.  Those early instructions will set up a mapping at the address where flash is eventually meant to reside, and jump there.

0 Kudos
Reply

2,464 Views
ravindrakulkarn
Contributor II

Thanks Scoot.

May I request you some more elaboration please.

However, The first instruction to be executed must be at address

0xFFFF_0x0100 according to the data sheet.

but the map file shows it at 0xEFF0_0100, then which code will map this

address (efff00100) to the real reset vector?

or am I missing something grossly?

Also I checked the linker command line, there is no change in start

instruction ( option "-e").

On Thu, Dec 6, 2012 at 12:15 AM, Scott Wood

0 Kudos
Reply

2,464 Views
scottwood
NXP Employee
NXP Employee

Just because the linker thinks an instruction is at 0xeff00100 doesn't mean it won't work when the code is actually located at 0xfff00100 -- except to the extent that any addresses contained in the code will point to the wrong place, but the early asm code is careful to avoid such problems.

The "early_bats" function establishes an effective-address mapping at 0xeff00000 that points to 0xfff00000, and then the code branches to an address in that region.  Later on the flash gets physically mapped at 0xeff00000.

0 Kudos
Reply

2,464 Views
ravindrakulkarn
Contributor II

Hi Scott

I find that the MPC8640 is actually getting to 0xFFF00800 address as against 0xFFFF0100 mentioned in the data sheets, Any clue? help why is this difference?

I am using USB TAP from Freescale , and there is no init script and default reset configuration, no Alt boot, no EEPROM.

Thanks

0 Kudos
Reply

2,464 Views
scottwood
NXP Employee
NXP Employee

The reset vector in the manual is 0xfff0_0100, not 0xffff_0100.  0xfff0_0800 is the floating point unavailable vector.  Are you sure that 0xfff0_0800 is the very first thing you see executed?  Maybe you've got a floating point instruction (or bad instruction that decodes as floating point) at 0xfff0_0100?

0 Kudos
Reply

2,464 Views
ravindrakulkarn
Contributor II

That was good help, Scott, Thanks

On Tue, Jan 15, 2013 at 11:52 PM, Scott Wood

0 Kudos
Reply