Request for product MPC5200CVR400B and PCF8582C-2T/03 reliability dat

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Request for product MPC5200CVR400B and PCF8582C-2T/03 reliability dat

1,810 Views
kyokozhu
Contributor I

I want to know  the MTBF or FIT value of  product MPC5200CVR400B and PCF8582C-2T/03 to do reliability prediction work 

Thank you very much!

 

2 Replies

1,643 Views
LPP
NXP Employee
NXP Employee

MTBF for PCF8582C is 3.33E8 Hours upon Tj=55 ºC at use conditions, activation energy of 0.7eV, and a 60% confidence level.

Reliability curves for MPC5200 are below.

MPC5200B_FIT.jpg

MPC5200B_MTTF.jpg

1,441 Views
nandhanuru
Contributor I

Hi,

Is there a linux driver available for PCF8582C EEPROM??

Or any other driver is compatible for PCF8582C?

Please help me with this information.

Thanks

 

 

0 Kudos
Reply