Today, for testing my nor flash driver in system, I erased 0XEFF00000 address accidentally;when I boot up the board later, the switch can not be connected but u-boot can also be used!
So, I want to get the vsc7385_load.bin and program it to the erased address。There is no simulation around. I want to use u-boot to download the firmware to ram first through tftpboot,and then use the flash command to program it in target address.
Please if someone have the vsc7385_load.bin or all nor flash boot image,send to me!
My board is:P1020RDB-PD,u-boot version:2013.01-dirty (Jan 09 2014 - 10:00:41
Thank you!