Today, for testing my nor flash driver in system, I erased 0XEFF00000 address accidentally;when I boot up the board later, the switch can not be connected but u-boot can also be used!
So, I want to get the vsc7385_load.bin and program it to the erased address。There is no simulation around. I want to use u-boot to download the firmware to ram first through tftpboot,and then use the flash command to program it in target address.
Please if someone have the vsc7385_load.bin or all nor flash boot image,send to me!
My board is:P1020RDB-PD,u-boot version:2013.01-dirty (Jan 09 2014 - 10:00:41
Thank you!
Solved! Go to Solution.
The binary is attached.
Also it is present in the NXP Linux SDK v.1.9 E500V2 IMAGE ISO.
For the image deployment refer to the QorIQ SDK 1.9 Documentation, Table 57: NOR Flash Memory Map P1020RDB-PD.
Your answer is helpful and thank you !