RGMII ping fails at U-boot T1022

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RGMII ping fails at U-boot T1022

5,633 次查看
rammurmu
Contributor III

We have a custom board based on T1022 processor, in the board there are two PHY [DP83867] connected to processor via RGMII port. When we ping the server from uboot then the FCS error is being reported in the tx packets using T32 debugging cable.

The "mii info" displays the two phys attached to the processor but ping is not working at uboot. Is this somekind of configuration error or configuration related to RGMII is missing?

U-BOOT log

---------------------------------------------------------------------------------------------------------------------------------------------------------------

Initializing....using SPD
Not enough bank(chip-select) for CS0+CS1 on controller 0, interleaving disabled!
2 GiB left unmapped
Loading second stage boot loader .................................................................................................

U-Boot 2016.012.0+ga9b437f (Nov 19 2018 - 05:41:10 +0530)

CPU0: T1022E, Version: 1.1, (0x85290211)
Core: e5500, Version: 2.1, (0x80241021)
Single Source Clock Configuration
Clock Configuration:
CPU0:1400 MHz, CPU1:1400 MHz,
CCB:600 MHz,
DDR:800 MHz (1600 MT/s data rate) (Asynchronous), IFC:150 MHz
QE:300 MHz
FMAN1: 600 MHz
QMAN: 300 MHz
PME: 300 MHz
L1: D-cache 32 KiB enabled
I-cache 32 KiB enabled
Reset Configuration Word (RCW):
00000000: 0c10000e 0e000000 00000000 00000000
00000010: 40000000 00400012 ec110000 21000000
00000020: 00000000 00000000 00000000 00038000
00000030: 00000000 c0165a05 00000000 00000000
I2C: ready
Board: T1022D4RDB
SPI: ready
DRAM: Detected UDIMM 76.XXXXX.XXX0B
Not enough bank(chip-select) for CS0+CS1 on controller 0, interleaving disabled!
4 GiB (DDR4, 64-bit, CL=11, ECC on)
L2: 256 KiB enabled
Corenet Platform Cache: 256 KiB enabled
Using SERDES1 Protocol: 64 (0x40)
SEC0: RNG instantiated
NAND: 1024 MiB
MMC: FSL_SDHC: 0
PLL read error 1
CCXK: Configure PLL FAILED
CCXK::PHY out of reset
SF: Detected N25Q512 with page size 256 Bytes, erase size 4 KiB, total 64 MiB
PCIe1: Root Complex, no link, regs @ 0xfe240000
PCIe1: Bus 00 - 00
PCIe2: Root Complex, no link, regs @ 0xfe250000
PCIe2: Bus 01 - 01
PCIe3: disabled
PCIe4: disabled
In: serial
Out: serial
Err: serial
SERDES Reference : 0x40
Net: Initializing Fman
SF: Detected N25Q512 with page size 256 Bytes, erase size 4 KiB, total 64 MiB
Fman1: Uploading microcode version 106.4.18
Could not get PHY for FSL_MDIO0: addr 0 2
Failed to connect
Could not get PHY for FSL_MDIO0: addr 0 2
Failed to connect
Could not get PHY for FSL_MDIO0: addr 0 7
Failed to connect
FM1@DTSEC1, FM1@DTSEC2, FM1@DTSEC3, FM1@DTSEC4, FM1@DTSEC5 [PRIME]
Hit any key to stop autoboot: 0
=> mii info
PHY 0x01: OUI = 0x80028, Model = 0x23, Rev = 0x01, 10baseT, HDX
PHY 0x04: OUI = 0x80028, Model = 0x23, Rev = 0x01, 10baseT, HDX
=> ping $serverip
FM1@DTSEC5 Waiting for PHY auto negotiation to complete......... TIMEOUT !
FM1@DTSEC5: No link.
Using FM1@DTSEC1 device

标签 (1)
标记 (1)
0 项奖励
回复
7 回复数

4,983 次查看
Pavel
NXP Employee
NXP Employee

There is the following in your message dump:

Could not get PHY for FSL_MDIO0: addr 0 2
Failed to connect
Could not get PHY for FSL_MDIO0: addr 0 2
Failed to connect
Could not get PHY for FSL_MDIO0: addr 0 7

 

Check you RGMII PHY addresses in u-boot configuration file.

onfiguration of the u-boot is available in the following folder in u-boot source: /include/configs/.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,983 次查看
rammurmu
Contributor III

Thanks for the reply Pavel . The PHY addressed were correctly mentioned in config file.

The issue was resolved by us. The issue was solved by modifying Line Interface Control Registers IF_Mode register of DPAA . The EN_Auto(automatic speed selection) and RG (RGMII) both the fields were enabled for the respective MAC.

Apart from this we also made changes in the PHY registers [RGMII Control Register (RGMIICTL), Address 0x0032]  to enable RGMII_TX_CLK_DELAY and RGMII_RX_CLK_DELAY fields.

0 项奖励
回复

4,983 次查看
anshulkhare
Contributor III

Hello rammurmu

in your Board in LInux kernel RGMII with DP83867 worked??

i am using SDK-V2.0-1701 which has linux kernel 4.1 where i am not getting TI Driver for DP83867

how did you configured RGMII in Linux kernel??

kindly help us to solve this issue.

RGMII with DP83867 in Linux Kernel for T2081 board 

Regards,

Anshul Khare

0 项奖励
回复

4,983 次查看
rammurmu
Contributor III

Get it work first in u-boot only. In our case the following changes helped

us find the solution-

========================================================================

The issue was resolved by us. The issue was solved by modifying Line

Interface Control Registers IF_Mode register of DPAA . The

EN_Auto(automatic speed selection) and RG (RGMII) both the fields were

enabled for the respective MAC.

Apart from this we also made changes in the PHY registers [RGMII Control

Register (RGMIICTL), Address 0x0032] to enable RGMII_TX_CLK_DELAY and

RGMII_RX_CLK_DELAY fields

================================================================================================================================================

RGMII configuration in kernel is just modifying the device tree entry to

incorporate RGMII.

Regards

Ram

On Wed, Mar 27, 2019 at 2:35 PM Anshul khare <admin@community.nxp.com>

0 项奖励
回复

4,983 次查看
anshulkhare
Contributor III

Hello rammurmu

Thanks for the reply.

in my case it is working in u-boot ,i am able to perform ping successfully and able to transfer file via TFTP.

it is having issue in Linux.

what modification is required in device tree to get it function properly.

Regards,

Anshul Khare

0 项奖励
回复

4,983 次查看
rammurmu
Contributor III

Please have a look at the RGMII entry in attached dts file.

Hope it will help you.

Regards

Ram

0 项奖励
回复

4,983 次查看
anshulkhare
Contributor III

Thank You

problem got solved 

issue was there in our device tree.

Regards,

Anshul Khare

0 项奖励
回复