Power management in MPC8640/41

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power management in MPC8640/41

699件の閲覧回数
amit123
Contributor I

Hello,

We have developed a custom board based on MPC8640D processor

In a board we are using serdes 1 - x8 PCIe and serdes 2 - SRIO port.

In temperature testing the processor resets at ambient 55 deg cel temperature testing with in 1 hour.

We have done 2 -3 iterations of the heat sink.

From processor point of view, I want to use and Implement  Dynamic frequency switching for Core, in order to reduce the power dissipation.

Kindly help how I can enable Dynamic frequency switching for MPC8640D

Regards,

Amit

0 件の賞賛
返信
1 返信

633件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Sorry, the device does not support Dynamic frequency switching


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信