PCI bus is not used in MPC8378

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCI bus is not used in MPC8378

1,033 次查看
rajeshanarasimh
Contributor I

Hi,

I am using MPC8378 processor in legacy design. MPC8378 PCI bus is not used in the design and all PCI Address lines were kept open in the design. We have initialized the RCWHR[PCIHOST] = 1 & RCWHR[PCIARB] = 1 in software. We haven't initialized the PCIACR[PM] = 1 or PCI_GCR[BBR] = 1 in software. Now we don't have opportunity to update the software. Is there any impact if we keep default value to PCIACR[PM] & PCI_GCR[BBR] in software?

Thanks for your support.

Regards,

Rajesh

Honeywell-Bangalore

0 项奖励
回复
2 回复数

953 次查看
r8070z
NXP Employee
NXP Employee

Have a great day,

PCIACR[PM] = 1 or PCI_GCR[BBR] set the PCI bus parked with the PCI controller when the MPC8378 drives PCI_AD[31:0] pins as outputs. So impact is that you may have float 32 inputs. These input signals are ignored if the PCI control inputs are terminated properly i.e. are in inactive state. However these floats inputs may increase power consumption and noise.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

953 次查看
rajeshanarasimh
Contributor I

Thanks for the reply. As per below e-mail, PCI pins will have noise. Are you suspecting emission or susceptible noise issue if we float these pins? Any failure reported due to these floating pins?

Thanks,

Rajesh

Honeywell-Bangalore

0 项奖励
回复