P1022: Serial file transfer via uboot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P1022: Serial file transfer via uboot

3,834 次查看
hemwant
Contributor IV

I am having a P1022 based board, i wanted to transfer the file using serial cable in uboot with command loady. As soon as transmission of file starts it gives NAK error on the prompt.

I am able to transfer the files using serial in linux using base64 utility.

Is there any configuration required in P1022 uboot to enable serial data transfer via UART cable?

0 项奖励
回复
3 回复数

3,826 次查看
ufedor
NXP Employee
NXP Employee

Please provide additional information:

1) U-Boot booting  and loady execution log (as text attachment)

2) which terminal client is used? Can you try Tera Term?

0 项奖励
回复

3,759 次查看
hemwant
Contributor IV

@ufedor 

 

1) U-Boot booting and loady execution log (as text attachment)

I have attached uboot console log in text file also the screenshot of loady error is attached.

 

2) which terminal client is used? Can you try Tera Term?

For now we are using minicom in linux. We are able to transfer the file with minicom in t1022 processor, mpc8260, mpc8569 .

0 项奖励
回复

3,752 次查看
ufedor
NXP Employee
NXP Employee

> We are able to transfer the file with minicom in t1022 processor, mpc8260, mpc8569 .

Corresponding U-Boot code was not modified for P1022.

0 项奖励
回复