P1010/P2020 1588v2 questions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1010/P2020 1588v2 questions

3,074件の閲覧回数
hansonhe
NXP Employee
NXP Employee

There is no TC/BC (Transparent Clock/Boundary Clock) in the 1588 register description of P1010/2020.

If TC mode needs to be supported, how should it be operated? Is software support enough for ptp4l?

Currently, this device is used as an ordinary clock and only as a Slave.

Is there any difference in the operation of the Slave when it is in a mode of TC or BC?

The IEEE1588 module of P1010/2020 does not process any PTP protocol messages, but only collects and processes them by CPU. Whether precision will deteriorate with the increase of system load?

Where can the PTP2 source code be obtained? Thanks.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,908件の閲覧回数
ufedor
NXP Employee
NXP Employee

IEEE1588 hardware assist unit in P1010/P2020 has provisions for all types of network clocks specified by IEEE1588v2.

However, it is only a hardware assist unit, not a complete clock implementation. To build a complete IEEE1588v2 network clock, software stack is required. Such complete solutions were developed by IXXAT.

0 件の賞賛
返信

2,913件の閲覧回数
hansonhe
NXP Employee
NXP Employee

uferdor, 

Thanks, whether we have similar SDK package or validation testing software on this IEEE1588v2 function?

0 件の賞賛
返信

2,912件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the Linux SDK Documentation:

Submit Form 

0 件の賞賛
返信