Not able to boot MPC8309TWR board through SD card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not able to boot MPC8309TWR board through SD card

1,433件の閲覧回数
jitenpatel
Contributor II
Hi all, 
We are working on MPC8309TWR board. We need to boot the board using SD card. 
Following are the changes we did for sdcard boot :-
Hardware specific:-
1) Modified switch settings of tower board to SW8(OB_BOOT)=1, that will make BOOT_CFG[0:3]=[1:1:0:1] for esdhc boot
2) Above step will put MPC8309 tower board to hard-coded RCW, boot from eSDHC (in this mode no RCW word required)
BSP specific (These changes are mentioned in the document http://cache.freescale.com/files/32bit/doc/app_note/AN3659.pdf ):-
1) Added macro to enable ramboot (CONFIG_SYS_RAMBOOT) 
2) Changed TEXT_BASE to 0x1000000 (ram address)
3) Also changed IMMR address (#define CONFIG_SYS_IMMR     0xFFF00000)
4) compile uboot and used uboot.bin file
5) now configuration file used for format sdcard is taken from the link provided by ufedor (https://community.nxp.com/thread/432611#comments )
6) used bootformat utility to format the sd card (./boot_format cfg_file_sd_mpc8309.DAT u-boot.bin -sd /dev/sdb)
Still we are not able to boot from SD card. Is there anything missing from the above configuration. How can we debug the sdcard boot method.
0 件の賞賛
返信
1 返信

1,158件の閲覧回数
usingbothmuxand
Contributor II

Hi jiten patel, 

Are you able to boot mpc8309twr from sd card. Please let me know if you have got any solution because I am also not able to boot mpc8309twr board with the above configurations u mentioned. 

0 件の賞賛
返信