We have two routers in same chassis. we need to test communication between 2 routers. we have 4 SGMII interfaces. 2 are connected between CPU-FPGA. Another SGMMI between two routers. currently we are using free scale processor T1040 and kernel 3.8.13. I have changed dts file as fallows. Once the system up on two machines I am trying to ping with eth2 (eth0 and eth1 are used by CPU-FPGA). But I am not getting any response. I am attaching 2 dts files,
Pass case:
fsl_mac: fsl_mac: FSL FMan MAC API based driver ()
fsl_mac ffb4e0000.ethernet: FMan MEMAC
fsl_mac ffb4e0000.ethernet: FMan MAC address: 00:22:bd:dd:e7:8a
fsl_mac ffb4e2000.ethernet: FMan MEMAC
fsl_mac ffb4e2000.ethernet: FMan MAC address: 00:04:9f:03:05:e5
fsl_mac ffb4e4000.ethernet: FMan MEMAC
fsl_mac ffb4e4000.ethernet: FMan MAC address: 00:00:04:9f:03:05
fsl_mac ffb4e6000.ethernet: FMan MEMAC
fsl_mac ffb4e6000.ethernet: FMan MAC address: 00:04:9f:03:05:e7
Fail case:
fsl_mac ffb4e0000.ethernet: of_get_mac_address(/soc@ffb000000/fman@400000/ethernet@e0000) failed
fsl_mac: probe of ffb4e0000.ethernet failed with error -22
fsl_mac ffb4e2000.ethernet: of_get_mac_address(/soc@ffb000000/fman@400000/ethernet@e2000) failed
fsl_mac: probe of ffb4e2000.ethernet failed with error -22
fsl_mac ffb4e4000.ethernet: of_get_mac_address(/soc@ffb000000/fman@400000/ethernet@e4000) failed
fsl_mac: probe of ffb4e4000.ethernet failed with error -22
fsl_mac ffb4e6000.ethernet: FMan MEMAC
fsl_mac ffb4e6000.ethernet: FMan MAC address: 00:04:9f:03:05:e7
fsl_dpa: FSL DPAA Ethernet driver ()
fsl_dpa ethernet.16: dev_get_drvdata(ffb4e0000.ethernet) failed
fsl_dpa: probe of ethernet.16 failed with error -22
fsl_dpa ethernet.17: dev_get_drvdata(ffb4e2000.ethernet) failed
fsl_dpa: probe of ethernet.17 failed with error -22
fsl_dpa ethernet.18: dev_get_drvdata(ffb4e4000.ethernet) failed
fsl_dpa: probe of ethernet.18 failed with error -22
fsl_dpa: fsl_dpa: Probed interface eth0
fsl_dpa_shared: FSL DPAA Shared Ethernet driver ()
fsl_dpa_proxy: FSL DPAA Proxy initialization driver ()
fsl_oh: FSL FMan Offline Parsing port driver ()
Other than dts file changes do I need to do changes in phy driver file to tweek eth2.
Original Attachment has been moved to: non-working.dts.txt.zip
Original Attachment has been moved to: working.dts.txt.zip
解決済! 解決策の投稿を見る。
Hi,
From the working .dts file provided, it seems sg.m3 is on MDIO bus:
mdio0: mdio@fc000 {
phy_sgmii_2: ethernet-phy@03 {
reg = <0x03>;
};
So my question is about the hardware, does Serdes lane B routed to PHY or to chasis?
Have a great day,
Lunmin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
after assigning ip address the link was up, but ping is failing. that is our requirement. as a said this one MAC-MAC
Please ignore earlier dts, Now i have modifed dts and made eth2 as fixed-link. it is coming up fine. I have pasted new dts at end.
Once the linux up if I use.
root@t1040rdb:/media/ram# ethtool eth2
Settings for eth2:
Supported ports: [ ]
Supported link modes: Not reported
Supported pause frame use: No
Supports auto-negotiation: No
Advertised link modes: Not reported
Advertised pause frame use: No
Advertised auto-negotiation: No
Speed: Unknown!
Duplex: Half
Port: Twisted Pair
PHYAD: 0
Transceiver: internal
Auto-negotiation: off
MDI-X: Unknown
Current message level: 0xffffffff (-1)
drv probe link timer ifdown ifup rx_err tx_err tx_queued intr tx_done rx_status pktdata hw wol 0xffff8000
Link detected: no
If I assign ip address
root@t1040rdb:/media/ram# ifconfig eth2 5.55.11.39
root@t1040rdb:/media/ram# route add default gw 5.55.0.1 eth2
root@t1040rdb:/media/ram# ethtool eth2
Settings for eth2:
Supported ports: [ MII ]
Supported link modes: 1000baseT/Full
Supported pause frame use: No
Supports auto-negotiation: Yes
Advertised link modes: 1000baseT/Full
Advertised pause frame use: No
Advertised auto-negotiation: Yes
Speed: Unknown!
Duplex: Unknown! (255)
Port: MII
PHYAD: 3
Transceiver: external
Auto-negotiation: on
Current message level: 0xffffffff (-1)
drv probe link timer ifdown ifup rx_err tx_err tx_queued intr tx_done rx_status pktdata hw wol 0xffff8000
Link detected: yes
ifconfig eth2
ifconfig eth2 5.55.11.39
route add default gw 5.55.0.1 eth2
ethtool eth2
ethtool -s eth2 autoneg off
ethtool eth2
netstat -rn
ping 5.55.11.34
Same process i am doing on other router but still ping failing between two routers
Current DTS file:
fman0: fman@400000 {
enet0: ethernet@e0000 {
fixed-link = <0 1 1000 0 0>;
phy-connection-type = "sgmii";
};
enet1: ethernet@e2000 {
fixed-link = <1 1 1000 0 0>;
phy-connection-type = "sgmii";
};
enet2: ethernet@e4000 {
fixed-link = <3 1 1000 0 0>;
phy-connection-type = "sgmii";
};
enet3: ethernet@e6000 {
phy-handle = <&phy_rgmii_0>;
phy-connection-type = "rgmii";
};
enet4: ethernet@e8000 {
phy-handle = <&phy_rgmii_1>;
phy-connection-type = "rgmii";
};
mdio0: mdio@fc000 {
phy_sgmii_2: ethernet-phy@03 {
reg = <0x03>;
};
phy_rgmii_0: ethernet-phy@01 {
reg = <0x01>;
};
phy_rgmii_1: ethernet-phy@02 {
reg = <0x02>;
};
};
};
};
fsl,dpaa {
compatible = "fsl,t1040-dpaa", "fsl,dpaa";
ethernet@0 {
compatible = "fsl,t1040-dpa-ethernet", "fsl,dpa-ethernet";
fsl,fman-mac = <&enet0>;
};
ethernet@1 {
compatible = "fsl,t1040-dpa-ethernet", "fsl,dpa-ethernet";
fsl,fman-mac = <&enet1>;
};
ethernet@2 {
compatible = "fsl,t1040-dpa-ethernet", "fsl,dpa-ethernet";
fsl,fman-mac = <&enet2>;
};
ethernet@3 {
compatible = "fsl,t1040-dpa-ethernet", "fsl,dpa-ethernet";
fsl,fman-mac = <&enet3>;
};
ethernet@4 {
compatible = "fsl,t1040-dpa-ethernet", "fsl,dpa-ethernet";
fsl,fman-mac = <&enet4>;
};
};
And you wrote:
"mdio0: mdio@fc000 {
phy_sgmii_2: ethernet-phy@03 {
reg = <0x03>;
}
This does not connected to PHY. It is connected to other RSP." ====> How? Please clarify to help understanding. Thanks.
So one router eth2 has ip 5. 55.11.39 and another is 5.55.11.34? What's eth3 dedicated for?
What's the interface of router to chassis? Can you please clarify this? Thanks.
Hi Lumin,
Thanks for your reply, we are using T1040 eval board dts file, because of that we have not done any clean up.
In the
phy_rgmii_0: ethernet-phy@01 {
reg = <0x01>;
};
This is for Marvell PHY.
as you asked
mdio0: mdio@fc000 {
phy_sgmii_2: ethernet-phy@03 {
reg = <0x03>;
}
This does not connected to PHY. It is connected to other RSP.
I have modified dts file in clean way. PFA. But with this dts also I am getting same error
fsl_mac ffb4e0000.ethernet: of_get_mac_address(/soc@ffb000000/fman@400000/ethernet@e0000) failed
fsl_mac: probe of ffb4e0000.ethernet failed with error -22
fsl_mac ffb4e2000.ethernet: of_get_mac_address(/soc@ffb000000/fman@400000/ethernet@e2000) failed
fsl_mac: probe of ffb4e2000.ethernet failed with error -22
fsl_mac ffb4e4000.ethernet: of_get_mac_address(/soc@ffb000000/fman@400000/ethernet@e4000) failed
fsl_mac: probe of ffb4e4000.ethernet failed with error -22
fsl_mac ffb4e6000.ethernet: FMan MEMAC
AS i said earlier we have 4 SGMII ports 2 SGMII ports connected to CPU to FPGA. 1 SGMII connected between 2 routers
include/ "fsl/t104xsi-pre.dtsi"
/ {
model = "fsl,T1040RDB";
compatible = "fsl,T1040RDB";
#address-cells = <2>;
#size-cells = <2>;
interrupt-parent = <&mpic>;
aliases {
phy_rgmii_0 = &phy_rgmii_0;
phy_rgmii_1 = &phy_rgmii_1;
phy_sgmii_2 = &phy_sgmii_2;
};
memory {
device_type = "memory";
};
dcsr: dcsr@f00000000 {
ranges = <0x00000000 0xf 0x00000000 0x01072000>;
};
bportals: bman-portals@ff4000000 {
ranges = <0x0 0xf 0xf4000000 0x2000000>;
};
qportals: qman-portals@ff6000000 {
ranges = <0x0 0xf 0xf6000000 0x2000000>;
};
soc: soc@ffb000000 {
ranges = <0x00000000 0xf 0xfb000000 0x1000000>;
reg = <0xf 0xfb000000 0 0x00001000>;
i2c@118100 {
pca9546@77 {
compatible = "philips,pca9546";
reg = <0x77>;
#address-cells = <1>;
#size-cells = <0>;
};
};
spi@110000 {
flash@0 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "micron,n25q512a";
reg = <0>;
spi-max-frequency = <10000000>; /* input clock */
};
};
fman0: fman@400000 {
enet0: ethernet@e0000 {
fixed-link = <0 1 1000 0 0>;
phy-connection-type = "sgmii";
};
enet1: ethernet@e2000 {
fixed-link = <1 1 1000 0 0>;
phy-connection-type = "sgmii";
};
enet2: ethernet@e4000 {
phy-handle = <&phy_sgmii_2>;
phy-connection-type = "sgmii";
};
enet3: ethernet@e6000 {
phy-handle = <&phy_rgmii_0>;
phy-connection-type = "rgmii";
};
enet4: ethernet@e8000 {
phy-handle = <&phy_rgmii_1>;
phy-connection-type = "rgmii";
};
mdio0: mdio@fc000 {
phy_sgmii_2: ethernet-phy@03 {
reg = <0x03>;
};
phy_rgmii_0: ethernet-phy@01 {
reg = <0x01>;
};
phy_rgmii_1: ethernet-phy@02 {
reg = <0x02>;
};
};
};
};
pci0: pcie@ffb240000 {
reg = <0xf 0xfb240000 0 0x10000>;
ranges = <0x02000000 0 0xe0000000 0x0 0xe0000000 0x0 0x10000000>;
};
pci1: pcie@ffb250000 {
reg = <0xf 0xfb250000 0 0x10000>;
ranges = <0x02000000 0 0xf0000000 0x0 0xf0000000 0 0x40000000>;
};
pci2: pcie@ffb260000 {
reg = <0xf 0xfb260000 0 0x10000>;
ranges = <0x02000000 0 0xe0000000 0x0 0x20000000 0 0x10000000>;
};
pci3: pcie@ffb270000 {
reg = <0xf 0xfb270000 0 0x10000>;
ranges = <0x02000000 0 0xe0000000 0x0 0xb0000000 0 0x10000000>;
};
fsl,dpaa {
compatible = "fsl,t1040-dpaa", "fsl,dpaa";
ethernet@0 {
compatible = "fsl,t1040-dpa-ethernet", "fsl,dpa-ethernet";
fsl,fman-mac = <&enet0>;
};
ethernet@1 {
compatible = "fsl,t1040-dpa-ethernet", "fsl,dpa-ethernet";
fsl,fman-mac = <&enet1>;
};
ethernet@2 {
compatible = "fsl,t1040-dpa-ethernet", "fsl,dpa-ethernet";
fsl,fman-mac = <&enet2>;
};
ethernet@3 {
compatible = "fsl,t1040-dpa-ethernet", "fsl,dpa-ethernet";
fsl,fman-mac = <&enet3>;
};
ethernet@4 {
compatible = "fsl,t1040-dpa-ethernet", "fsl,dpa-ethernet";
fsl,fman-mac = <&enet4>;
};
};
};
/include/ "fsl/t1040si-post.dtsi"
/include/ "fsl/qoriq-dpaa-res3.dtsi"
One more question, for the working.dts you provided, do you mean all those links are up, or you can ping from one router to another on eth2?
Hi,
You wrote "We have two routers in same chassis."
and
"mdio0: mdio@fc000 {
phy_sgmii_2: ethernet-phy@03 {
reg = <0x03>;
}
This does not connected to PHY. It is connected to other RSP.
"
Then what's the interface to other RSP? The interface on the chassis? Are you using two identical routers? which is based on T1040. Please provide more detail information. A graphic may be useful.
Regards
Lunmin
Hi,
Is this dts the one after you modified? "I have modified dts file in clean way".
Have a great day,
Lunmin
Hi,
From the working .dts file provided, it seems sg.m3 is on MDIO bus:
mdio0: mdio@fc000 {
phy_sgmii_2: ethernet-phy@03 {
reg = <0x03>;
};
So my question is about the hardware, does Serdes lane B routed to PHY or to chasis?
Have a great day,
Lunmin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------