If I try to connect MPC8245 by USB TAP,then Codewarrior will give me a error report,picture1;
When I cancel the option of"reset Target on lanuch"in Remote Debugging Tabe ,then ,It will give me a select dialog box,picture2
if i click "No",it will be picture3;
I use two 16bit SDRAM(IS42S16800F) as 32 BIT data width;and My initialization configration file as picture4 and picture5(rewrite from a sandpoint configration file);
I don't know what is wrong? How should I do? Thanks.
Today,I found that the configration file is written in little-endian,but my cpu work on big-endian,so,I have change it to big-endian,but the same result.when I cancel the"reset target on launch"and click the"yes"button in dialog box,then,it will say:"error resetting target from initialization file". So I think,My inintialization file is something wrong,If you could give me some demo for MPC8245 or some spcification,thanks.
As far as I remember, CodeWarrior USB TAP debug probe does not support MPC8245 device working in 32-bit bus mode.
The only 64-bit mode is supported. For 32-bit mode you have to use another debug probe.
Please double check with CodeWarrior team.
Have a great day,
Alexander
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------