MPC8572E BringUp Guide

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8572E BringUp Guide

1,306 Views
alicankurutepe
Contributor II

Hello all,

We have a design with  the processor MPC8572E and have some problems with the low temperature tests(-40 celsius).

While digging the documents(errata mainly) we found that in the bring up guide(AN3647, Rev2) in section 1.7 table 1, we cannot see the our chip's device marking.

We two different chips that have the following device markings:

04M20X and 44M20X

Do you have a new version of this bring up guide or which revision of the MPC8572E have these device markings ?

Thanks in advance

Edit:

In the chip errata(MPC8572ECE Rev.N, 06/12) at page 39 it says:

A-004508: DDR controller may not function across the full industrial temperature range

Affects: DDR

Decription: When the DDR controller is initialized below 0 C and operated beyond am ambient tempature of 60 C, the DDR controller may not function properly.

Impact: Data corruption may be observed during reads from DRAM.

Workaround: When the DDR controller operates across the full supported industrial temperature range then software should set bit 22 at the CCSR register offset 0x0_2F08 before the DDR controller is enabled.

Fix Plan: No plans to fix.

This errata seems a way to fix the issue however in the family reference manual there is not such a register with the given offset. Anybody have an idea ?

Labels (2)
0 Kudos
Reply
1 Reply

1,135 Views
r8070z
NXP Employee
NXP Employee

Hello,

Rev. 2 is the last revision of the MPC8572e bring-up guide. The last qual report
https://www.google.ru/search?client=opera&q=16395_MPC8572_Qualification_Report_Rev_3_042214.pdf
mentions 04M20X for the MPC8572E rev. 2.2.1 You may check device part number instead of mask on the nxp site.

This register exists; it is just is not published. Also there was PCN
http://www.nxp.com/assets/documents/data/en/product-change-notices/PCN15248.htm
which says that customers need to implement the software workaround if their products need a DDR controller to operate over the entire lower extended temperature range.

0 Kudos
Reply