MPC8358 DDR2 ECC Registered

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8358 DDR2 ECC Registered

ソリューションへジャンプ
2,364件の閲覧回数
Amit24
Contributor I

Hi we have used  MPC8358 in our design a 5 year ago. Now, we are facing a problem shortage of DDR2 SDRAM ECC registered buffered.So Anyone cal able to tell me, Can we replace or design a new board with Standard SODIMM unbuffered DDR2  or with discrete chips.

Regrads

Amit Kumar

0 件の賞賛
返信
1 解決策
2,351件の閲覧回数
r8070z
NXP Employee
NXP Employee

Yes you can.
The MPC8360 reference manual says: The fully programmable DDR SDRAM controller supports most JEDEC standard ×8, ×16, or ×32 DDR2 and DDR memories available. In addition, unbuffered and registered DIMMs are supported. However, mixing different memory types or unbuffered and registered DIMMs in the same system is not supported. It also provides supported configurations

r8070z_1-1623071679923.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,292件の閲覧回数
Amit24
Contributor I

Hi,

Can i use 240 pin memory module with this ? if anyone have some resources , please share .

 

Thanks

Amit 

 

0 件の賞賛
返信
2,343件の閲覧回数
Amit24
Contributor I

Thanks for feedbck,Do you have reference circuit interfacing SODIMM or dicrete SDRAM chips?

Please share if you have.

Regards

Amit

0 件の賞賛
返信
2,352件の閲覧回数
r8070z
NXP Employee
NXP Employee

Yes you can.
The MPC8360 reference manual says: The fully programmable DDR SDRAM controller supports most JEDEC standard ×8, ×16, or ×32 DDR2 and DDR memories available. In addition, unbuffered and registered DIMMs are supported. However, mixing different memory types or unbuffered and registered DIMMs in the same system is not supported. It also provides supported configurations

r8070z_1-1623071679923.png

 

0 件の賞賛
返信
2,346件の閲覧回数
Amit24
Contributor I
 
0 件の賞賛
返信
2,334件の閲覧回数
r8070z
NXP Employee
NXP Employee

Check MPC8360EMDS: MPC8360EA Modular Development System page

https://www.nxp.com/design/qoriq-developer-resources/mpc8360ea-modular-development-system:MPC8360EMD...

I provides some design resources, including schematics of board with DDR2 SODIMM

https://www.nxp.com/downloads/en/schematics/MPC8360EAMDSSCH.pdf

0 件の賞賛
返信