MPC8315E - PCIe interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC8315E - PCIe interface

跳至解决方案
1,776 次查看
airazusta
Contributor II

Hello,

I was wondering how I should disable/enable the SerDes PCIe interface of the MPC8315E via SW.  Would be enough to configure SDPD bit of SRDSCR0 register to '1' (Block power down) for disable it? 

And should I also make any change in HW? For example, following the application note AN3438, it says that SD_IMP_CAL_TX signal has to be connected to GND using a 100R precision resistor when the interface is used, but when not used it has to be connected to 1V. If I disable the PCIe interface via SW, can SD_IMP_CAL_TX signal still be connected to the 100R resistor?

Thanks in advance!

Regards,

Ane

0 项奖励
回复
1 解答
1,677 次查看
Bulat
NXP Employee
NXP Employee

I believe it will be ok. Side effect is that grounded resistors could cause additional unnecessary power consumption.

Regards,

Bulat

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,677 次查看
Bulat
NXP Employee
NXP Employee

Yes, setting of SRDSCR0[24] bit is enough for powering down (disabling) entire SERDES from SW point of view.

Yes, if SERDES is not used, you can connect both SD_IMP_CAL_TX (and SD_IMP_CAL_RX) to 1V via 100 Ohm resistors.

Regards,

Bulat

1,677 次查看
airazusta
Contributor II

Thank you for answering Bulat!

And would it be ok if I leave both calibration signals connected to GND via 100 Ohm (or 200 Ohm) resistor when I power down the SERDES?

Regards,

Ane 

0 项奖励
回复
1,678 次查看
Bulat
NXP Employee
NXP Employee

I believe it will be ok. Side effect is that grounded resistors could cause additional unnecessary power consumption.

Regards,

Bulat

0 项奖励
回复