MPC8309 eLBC UPM mode customization.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC8309 eLBC UPM mode customization.

1,517 次查看
avinashpisal
Contributor I

Hi all,

      I am interfacing MPC8309 eLBC bus with FPGA in UPM mode,timing and functional information provided in reference manual is with respective to DRAM interface,

so would like to know,is it possible to configure UPM mode in simple read/write address and control signals format without DRAM compatible interface.

Thank you.

0 项奖励
回复
2 回复数

1,169 次查看
LPP
NXP Employee
NXP Employee

UPM functionality is not limitted to make DRAM interface only. It is flexible to support various I/O interfaces (SRAM, SSRAM...).

Usefull links:

Application Note "PowerQUICC UPM Configuration" + GUI  tool.

http://cache.freescale.com/files/32bit/doc/app_note/AN2810.pdf
http://www.freescale.com/webapp/sps/download/license.jsp?colCode=AN2810SW.ZIP

Compact Flash Interface Design

http://cache.freescale.com/files/32bit/doc/app_note/AN2647.pdf

Programming the User-Programmable Machine (UPM) for SDRAM  Memory Devices

http://cache.freescale.com/files/32bit/doc/app_note/AN3533.pdf


How to Interface NAND with UPM

http://cache.freescale.com/files/32bit/doc/white_paper/NANDFLASHWP.pdf

1,169 次查看
avinashpisal
Contributor I

Thank you for quick reply,

i will go through the links you have share here.

0 项奖励
回复