MPC8309 clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC8309 clock

跳至解决方案
1,518 次查看
qnb2013
Contributor I

Hi All, I am working on Freescale's TWR-MPC8309 board, I know about the reset configuration words(RCWLR and RCWHR) control the clock, but I hard to understand that when the reset configuration words are writed to Flash? if I want to modify the system bus clock, what should I do? Can The coherent system bus clock(csb_clk) be modified? Thanks!

0 项奖励
回复
1 解答
1,376 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

The MPC8309 has configuration inputs CFG_RESET_SOURCE[0:3] which are sampled on PORESET negation. The sampled value selects whether the device loads a reset configuration word from NOR Flash, NAND Flash, or an I2C EEPROM or uses hard-coded default options. Also debugger connected to the MPC8309 JTAG port can configure device. So there are options when device can start without RCW in the NOR flash.

Notice when you already have RCW and U-boot in the NOR flash you can rewrite the flash content in order to change the RCW. U-boot provides commands for common flash operations such as: reading sectors, erasing sectors, writing sectors, sector protecting. But take into account it is dangerous operation - you should not write invalid RCW or corrupt U-boot.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,377 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

The MPC8309 has configuration inputs CFG_RESET_SOURCE[0:3] which are sampled on PORESET negation. The sampled value selects whether the device loads a reset configuration word from NOR Flash, NAND Flash, or an I2C EEPROM or uses hard-coded default options. Also debugger connected to the MPC8309 JTAG port can configure device. So there are options when device can start without RCW in the NOR flash.

Notice when you already have RCW and U-boot in the NOR flash you can rewrite the flash content in order to change the RCW. U-boot provides commands for common flash operations such as: reading sectors, erasing sectors, writing sectors, sector protecting. But take into account it is dangerous operation - you should not write invalid RCW or corrupt U-boot.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,376 次查看
qnb2013
Contributor I

Thank you for help me!

How to ascertain the address of RCW  in the NOR Flash if I rewrite the flash content. I know the 32M NOR flash starts at address 0xFE000000, the location for U-Boot is fixed(0xfe00_000--0xfe09_ffff)。

the 32M NOR flash contents:

0xfe00_0000 - 0xfe09_ffff      U-Boot

0xfe0e_0000 - 0xfe0f_ffff       DTB

0xfe10_0000 - 0xfe3f_ffff       Kernel

0xfe7e_0000 - 0xfe7e_ffff      QE ucode

0xfe80_0000 - 0xfeff_ffff        Ramdisk file system

where does the device loads a reset configuration word from NOR Flash?

0 项奖励
回复