MPC8309 SD/MMC/SPI Boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8309 SD/MMC/SPI Boot

1,177件の閲覧回数
ganjiaravind
Contributor I

Hi everyone ,when MPC8309twr Board need to Boot from SD/MMC or SPI device there should be a configuration dat file,among all configuration offsets i have a question over the offsets 0x50,0x58,0x60.

offset 0x50 ---- Source address

offset 0x58 ---- Target address

offset 0x60 ---- Execution starting address

what exact values to be used in this offsets or is there any procedure to calculate ,

thank you in advance.

0 件の賞賛
返信
1 返信

996件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

Please check Booting with sd card in MPC8309twr It provides example of the dat file.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信