MPC8280 SDRAM 60x Bus按顺序写出错

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8280 SDRAM 60x Bus按顺序写出错

718 Views
lhb_will
Contributor IV

在外面集成了两块SDRAM,型号是MT48LC4M32B2-。但是按照顺序向0地址写0x00000000,1地址写0x11111111,2地址写0x22222222,3地址写0x33333333,4地址写0x4444444,以此类推,数据写到0xffffffff后重新写入数据0x00000000.

但是SDRAM的数据写完后成如下状况,地址里的数据和预期的不一致。请问可能是哪里的原因?

1706341401.jpg

0 Kudos
1 Reply

627 Views
Pavel
NXP Employee
NXP Employee

Perhaps some address lines are short-circuited on your board.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------