MPC8270 Patch Prerequisites

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC8270 Patch Prerequisites

跳至解决方案
1,382 次查看
sai_jagannathan
Contributor II

We are about to migrate from MPC8260 to MPC8270. We plan to use the microcode patch that needs to be included for the MPC8270 to resolve ethernet related issues. Is there a prerequisite for the patch to be applied? example FCC driver to be started before patch to be applied? or can it be applied as soon as processor is out of reset.

标记 (1)
0 项奖励
回复
1 解答
1,264 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,


The microcode patch can  be applied as soon as processor is out of reset.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,265 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,


The microcode patch can  be applied as soon as processor is out of reset.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,264 次查看
sai_jagannathan
Contributor II

Hi Serguei, 

Is there a way to find if the patch is running or not? 

Other than inspecting internal RAM address where it is loaded.

 

0 项奖励
回复