MPC8270 Patch Prerequisites

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8270 Patch Prerequisites

Jump to solution
1,315 Views
sai_jagannathan
Contributor II

We are about to migrate from MPC8260 to MPC8270. We plan to use the microcode patch that needs to be included for the MPC8270 to resolve ethernet related issues. Is there a prerequisite for the patch to be applied? example FCC driver to be started before patch to be applied? or can it be applied as soon as processor is out of reset.

Tags (1)
0 Kudos
Reply
1 Solution
1,197 Views
r8070z
NXP Employee
NXP Employee


Have a great day,


The microcode patch can  be applied as soon as processor is out of reset.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,198 Views
r8070z
NXP Employee
NXP Employee


Have a great day,


The microcode patch can  be applied as soon as processor is out of reset.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,197 Views
sai_jagannathan
Contributor II

Hi Serguei, 

Is there a way to find if the patch is running or not? 

Other than inspecting internal RAM address where it is loaded.

 

0 Kudos
Reply