MPC8270 PCI Bridge Configuration Register offset 0x40 and 0x98

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8270 PCI Bridge Configuration Register offset 0x40 and 0x98

Jump to solution
1,588 Views
reedy
Contributor III

While making modifications to legacy software we have found writes to reserved/undocumented registers.  Maybe these are from an early datasheet or errata?

Both writes are to the host PCI configuration space (bus=0, dev=0, fxn=0)

// PCI Bridge Option

0x40 = 0x00000004;

// PCI PIMOSA

0x98 = 0xC0000003;


Does anyone recognize what these register writes are doing?

Thanks,

0 Kudos
Reply
1 Solution
1,349 Views
Bulat
NXP Employee
NXP Employee

Those registers are definitely not from the MPC8270 PCI configuration space. If your software was really written for the MPC8270, you should remove those writes.

Regards,

Bulat

View solution in original post

0 Kudos
Reply
1 Reply
1,350 Views
Bulat
NXP Employee
NXP Employee

Those registers are definitely not from the MPC8270 PCI configuration space. If your software was really written for the MPC8270, you should remove those writes.

Regards,

Bulat

0 Kudos
Reply