MPC8260a 60x SDRAM external address multiplixer in 60x-compatible mode?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC8260a 60x SDRAM external address multiplixer in 60x-compatible mode?

4,621 次查看
mengjunling
Contributor I

Hi,everyone, I use MPC8260A in my design, now I encounter some problems when debugging. When I access SDRAM in CodeWarrior unsing USB-TAP, an error message "writemem on target failed at address 0x400, size 0x1000". But when I only access 0x100 bytes, it's ok.  I measure signal waveform using DPO,  the timing is correct.


Sometimes I refresh data in codewarrior, the memory data will change. It seems the refresh timing is wrong.


MPC8260 is in 60x-compatible mode,66Mhz bus clock . 60x SDRAM is configured 32bit-port ,128MB(13 rows, 10cols,4 bank, 512Mb density), page-based mode.   So 60x SDRAM address is latched and muxed externally. Please help me to check the address connection?

BR: MS = 60x SDRAM, Port size = 32bit

OR: BPD = 01(4 bank), row start = A5, row number = 13

PSDMR:PBI = 1, SDAM = 100, BSAM = 010(A14-A16)

SDRAM BA[1:0] using dedicated pin BNKSEL[1:2].

  row         bank-sel         col

A[5:17],  A[18:19],   A[20:29]

SDRAM pins: BA1    BA0              A12    A11     A10     A9----A0

Phsical  :      A15    A16               A17    A18     A19     A20---A29

ACT    :      BNKSEL1 BNKSEL2    A5      A6     SDA10  A9--- A17

R/W     :     BNKSEL1 BNKSEL2     --       --       AP       A20--A29  


60x address is muxed (using IDTQS3257): 

未命名.bmp

0 项奖励
回复
14 回复数

4,257 次查看
Bulat
NXP Employee
NXP Employee

You mentioned just a few fields of the PSDMR, can you let me know full PSDMR value?

0 项奖励
回复

4,257 次查看
mengjunling
Contributor I

PSDMR:PBI = 1, SDAM = 100, BSAM = 010(A14-A16), SDA10 = 011(A7), RFRC = 6 cycle, PRETOACT = 3, ACTTORW = 2 , BL = 1(8 bytes),  LDOTOPRE = -2, WRC =  2, EAMUX  = 1, BUFCMD  = 1, CAL  =  10(2),  .

The command bit changes with command being issued,  After issuing LOAD MODE REGISTER command,  RFEN bit is set.



0 项奖励
回复

4,257 次查看
Bulat
NXP Employee
NXP Employee

Try to set PSDMR[LDOTOPRE] = -1, instead of -2.

And let me know whether this helps.


0 项奖励
回复

4,257 次查看
mengjunling
Contributor I

I have set PSDMR[LDOTOPRE] = -1,

I found the problem, the PSDMR[CL] field is not the same as value written by LOAD MODE REGISTER command, because in 60x-compatible mode , the LOAD MODE REGISTER value must be calaulted by user software.  The software can run in SDRAM.

But I have a new problem when using USB_TAP.  Now when I access SDRAM 0x200@0x0 size using Codewarrior Debug-> EPPC -> fill memory, then View memory, only the first 0x100 bytes space is filled and the beginning address(0x0-0x5) is not written, and the second 0x100 byte is not filled.

But when I fill memory every 0x100 bytes, all data is written and ok.

If the SDRAM is still is not configured properly. the software can't run from SDRAM.  I dont know why.

0 项奖励
回复

4,257 次查看
Bulat
NXP Employee
NXP Employee

Can you check and provide a piece of initialization code where LOAD MODE REGISTER command is issued to the SDRAM?

0 项奖励
回复

4,257 次查看
mengjunling
Contributor I

And one more problem.

SMC is configured in UART,  I use the Demo Board SMC initilization code, but the SMC TXD pin outputs nothing. I turn LED after the SMC configuration, then I view register in Codewarrior,

the I/O port is configured right, but register CPCR / BRGC1/ SMC1MR is all zero(not the right value),

I want to know if the SDRAM is not working properly,  SMC initilization may be affected?

0 项奖励
回复

4,257 次查看
Bulat
NXP Employee
NXP Employee

I do not think that non-functional SDRAM can affect initialization of the SMC. However this can be code dependent, try to use a debugger to trace if SMC registers are really set during initilaization.

0 项奖励
回复

4,257 次查看
mengjunling
Contributor I

Now I chose the MPC8260A(266/166/66Mhz),  the CPM can run up to 166Mhz.

After I only change the CPM frequency from 166Mhz to 133Mhz by configuration word and MODCK[1:3] ,  the SMC works and ouputs properly.

I dont know why? 

0 项奖励
回复

4,257 次查看
mengjunling
Contributor I

The following is my initilization code using C code.  I port the code from one Demo , and work properly.  The only difference : Demo(64 bit port) in single-CPU mode ,but my board in 60x-compatible mode.

*ramaddr = 0x00000000;

M8260_PSRT(immrVal) = 0xB;

M8260_BR1(immrVal) = 0x00001841;

M8260_OR1(immrVal) = 0xF8002Bb00;

M8260_PSDMR(immrVal) = 0xAC4E277F; // Prechage

*ramaddr = 0xFF;

M8260_PSDMR(immrVal) = 0x8C4E277F;// CBR

for(i = 0, i<8;i++)

     *ramaddr = 0xFF;

M8260_PSDMR(immrVal) = 0x9C4E277F;

*(ramaddr + 0xCC) = 0xFF;

M8260_PSDMR(immrVal) = 0xC44E277f;

*ramaddr = 0xFF;

Thanks.

0 项奖励
回复

4,257 次查看
Bulat
NXP Employee
NXP Employee

Can you check if line

M8260_OR1(immrVal) = 0xF8002Bb00;

is exact copy from the code?

And one more question about address connection to the SDRAM. Do you have address latch prior to address multiplexer?

0 项奖励
回复

4,257 次查看
mengjunling
Contributor I

Yes, copy the code from Demo, but because the SDRAM port is not same, so OR1 is not totally same as Demo, 

I have address latch(16373) prior to address multiplexer.

0 项奖励
回复

4,257 次查看
Bulat
NXP Employee
NXP Employee

If (M8260_OR1(immrVal) = 0xF8002Bb00) is really used in the code, it can cause a problem. Value 0xF8002Bb00 (that is 0xF_8002_Bb00) seems to be mistaken, it contains 36 bits instead of 32 ones, so 4 upper bits are lost. Try to check its bit pattern against description in the Manaul.

0 项奖励
回复

4,257 次查看
mengjunling
Contributor I

Thank you!

I check the code once again.

0 项奖励
回复

4,257 次查看
mengjunling
Contributor I

Yes, I will try it.

Thanks!

0 项奖励
回复