We have an MPC7448-based board where the '7448 is waking up dead. No bus activity. We connected a Green Hills Probe (GHP) via JTAG, but from the GHP's vb command, it appears that TDO is either driven high or tri-stated (it's pulled up on the board).
The only visible activity is that CKSTP_OUT is negated (high) while HRESET is asserted; then as soon as HRESET is negated, CKSTP_OUT asserts, which I assume means that it had a checkstop/machine check immediately after coming out of reset.
I can't find any likely cause for a machine check before the first bus cycle. It appears that most causes have to be explicitly enabled, or at least occur during a memory access. If there are other "implementation-dependent" causes, I can't find anything on them.
I should mention that this is one out of a number of working boards of the same design, so it's likely a manufacturing issue. But I still need to find the cause. We've checked the power rails, input clock, resets - just about everything we can access.
Has anyone seen anything like this?