Linux driver for UMCC device on LS1043A or similar

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux driver for UMCC device on LS1043A or similar

4,006 Views
SteveMans
Contributor II

Is there a Linux driver for running the QUICC Engine UCC device in UMCC mode ?
We are aware of fsl_ucc_hdlc but we need a driver to run in UMCC mode

0 Kudos
Reply
7 Replies

3,932 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello @SteveMans 

Regarding your case request,

We do not have a driver available for LS1043A, since we have a few issues on it, nevertheless based on our LSDK, the driver available was originally created for P1021, you can use it as a base for create your own driver or you can contact our paid professional support services at the following link:

https://www.nxp.com/support/support/nxp-engineering-services/professional-support-for-processors-and...

Have a great day.

BR,

Hector Villarruel

0 Kudos
Reply

3,918 Views
SteveMans
Contributor II

How can I get that driver you refer to ? 
Is it available on the web ?

0 Kudos
Reply

3,891 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello @SteveMans 

Regarding your last reply,

How can I get that driver you refer to ? 
Is it available on the web ?

This driver is available on the LSDK.

BR,

Hector Villarruel

0 Kudos
Reply

3,695 Views
SteveMans
Contributor II

Thankyou for the reply.
I have looked in the LSDK but have not been able to find anything.
Please can you tell me exactly where the files I need are located, and what they are named.

Many thanks.

0 Kudos
Reply

3,607 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello @SteveMans 
Hope this post finds you well,

Regarding your last reply:

The drivers are available on the LSDK, I would also like to provide you with the following git where you can find the available drivers at the "drivers "section.

https://github.com/nxp-qoriq/linux

Nevertheless referring to my previous reply:

Please note that we do not have a driver available for LS1043A, since we have a few issues on it, nevertheless based on our LSDK, the driver available was originally created for P1021, you can use it as a base for create your own driver or you can contact our paid professional support services at the following link:

https://www.nxp.com/support/support/nxp-engineering-services/professional-support-for-processors-and...

Have a great day

BR,

Hector Villarruel

 

0 Kudos
Reply

3,216 Views
SteveMans
Contributor II

We have searched in the sdk but we cannot find anything resembling that driver.

If there really is a driver which exists for the P1021, then please can you tell me exactly where the files I need are located, and what they are named.

In other words, what is the actual filename which you are referring to ?

Many thanks 

 

 

0 Kudos
Reply

3,973 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello @SteveMans 

Hope this post finds you well,

This post is to inform you that we acknowledge the receipt of your case,
I Keep working on the solution on this case.
I’ll keep you informed on the process,

Have a great day.

BR,

Hector Villarruel

0 Kudos
Reply