Linux Folder is Missing in LTIB Build

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Linux Folder is Missing in LTIB Build

1,126 次查看
narreddiprakash
Contributor II

Hello,

            I am using LTIB for the kernel image generation for the board MPC8360EA-MDS-PB. I built the images successfully but the problem is that I couldn't find the directory "linux" in the path "../<ltib>/rpm/BUILD/linux". I checked the log of "./ltib --configure" where I found that the script removing this "linux" directory and the log is as follows..

Processing: kernel-2.6.22-mpc8360epb-rev2.1
======================
.
.
.
.
.
Processing files: kernel-2.6.22-2
Finding Provides: (using /opt/freescale/ltib/usr/lib/rpm/find-provides)...
Finding Requires: (using /opt/freescale/ltib/usr/lib/rpm/find-requires)...
PreReq: rpmlib(PayloadFilesHavePrefix) <= 4.0-1 rpmlib(CompressedFileNames) <= 3.0.4-1
Requires(rpmlib): rpmlib(PayloadFilesHavePrefix) <= 4.0-1 rpmlib(CompressedFileNames) <= 3.0.4-1
Wrote: /home/rnd/Desktop/8360/ltib-mpc8360epb-20081112/rpm/RPMS/ppc/kernel-2.6.22-2.ppc.rpm
Executing(%clean): /bin/sh -e /home/rnd/Desktop/8360/ltib-mpc8360epb-20081112/tmp/rpm-tmp.37360
+ umask 022
+ cd /home/rnd/Desktop/8360/ltib-mpc8360epb-20081112/rpm/BUILD
+ cd linux-2.6.22
+ rm -rf /home/rnd/Desktop/8360/ltib-mpc8360epb-20081112/tmp/kernel
+ [ -z ]
+ rm -f /home/rnd/Desktop/8360/ltib-mpc8360epb-20081112/rpm/BUILD/linux
+ exit 0
Executing(--clean): /bin/sh -e /home/rnd/Desktop/8360/ltib-mpc8360epb-20081112/tmp/rpm-tmp.37360
+ umask 022
+ cd /home/rnd/Desktop/8360/ltib-mpc8360epb-20081112/rpm/BUILD
+ rm -rf linux-2.6.22
+ exit 0
Build time for kernel-2.6.22-mpc8360epb-rev2.1: 386 seconds

sudo /opt/freescale/ltib/usr/bin/rpm --dbpath /home/rnd/Desktop/8360/ltib-mpc8360epb-20081112/rpmdb -e --allmatches --nodeps kernel 2>/dev/null
sudo /opt/freescale/ltib/usr/bin/rpm --dbpath /home/rnd/Desktop/8360/ltib-mpc8360epb-20081112/rpmdb --prefix /home/rnd/Desktop/8360/ltib-mpc8360epb-20081112/rootfs --ignorearch -ivh --force --excludedocs /home/rnd/Desktop/8360/ltib-mpc8360epb-20081112/rpm/RPMS/ppc/kernel-2.6.22-2.ppc.rpm
error: failed to stat /home/rnd/.gvfs: Permission denied
Preparing... ########################################### [100%]
1:kernel ########################################### [100%]

How can I edit this script to not to remove that directory.? Where from the "./ltib --configure" starts its building.?

Please, respond as soon as possible.

Thanks and Regards,

Prakash Reddy

标记 (1)
0 项奖励
回复
1 回复

1,029 次查看
Pavel
NXP Employee
NXP Employee

Use the following commands

 

Usually the following command sequence is used for kernel building under LTIB.

  1. ./ltib – This command is used for LTIB building

 

2. ./ltib -m prep -p kernel - This command is used for getting kernel source.Change the kernel configuration. 3. ./ltib -m scbuild -p kernel - This command is used for building the kernel. 4. ./ltib -m scdeploy -p kernel - This command provides deploying the kernel. See please the following pages:http://www.bitshrine.org/autodocs/LtibFaq.html


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------