LS1046A heatsin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046A heatsin

2,092件の閲覧回数
Nareshvarikuntla
Contributor III

Dear NXP,

We would like to add heat sink on LS1046A and this heat sink will be connected to chassis. We would like to maintain Isolation between the chassis and LS1046S GND pins.

So I would like to know LS1046A metal case is connected to GND pins or not. If not connected, how much isolation is between GND pins and LS 1046A metal case.

Regards,

Naresh V.

タグ(3)
0 件の賞賛
返信
1 返信

2,085件の閲覧回数
ufedor
NXP Employee
NXP Employee

The lid is connected to the back of the die with thermal interface material and the foot of the lid attached down to substrate with epoxy. No tie in to ground

Nevertheless it is needed to use thermal interface material between heatsink and the lid - refer to the QorIQ LS1046A, LS1026A Data Sheet, Figure 91. Package exploded, cross-sectional view-FC-PBGA.

0 件の賞賛
返信