Iwhetstone result on p2020

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Iwhetstone result on p2020

1,086 Views
djw1987419
Contributor I

i usr the whetstone to test my p2020, The result of Double Precision is only 0.123 mflous/mhz, so slow?Is there an optimized project for whetston on p2020?

0 Kudos
Reply
1 Reply

1,036 Views
alexander_yakov
NXP Employee
NXP Employee

We do not offer official Whetstone numbers for P2020 processor, so there is no "reproducibility guide" or ready to use Whetstone project available.

Have a great day,
Alexander,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply