Is there any IBIS model for p2020?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any IBIS model for p2020?

1,222件の閲覧回数
djw1987419
Contributor I

Is there any IBIS model for p2020? I couldn't find it on NXP website?

0 件の賞賛
返信
1 返信

1,142件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

The P2020 IBIS model can be provided under non-disclosure agreement (NDA) only. To obtain additional information please create a Technical Case:

https://community.nxp.com/thread/381898

-------------------------------------------------------------------------------
Note:
This thread is continued as a private discussion with the submitter,
NXP support is not following the thread anymore
-------------------------------------------------------------------------------

0 件の賞賛
返信