I have a question about TAP reset of MPC 866 (JTAG).

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I have a question about TAP reset of MPC 866 (JTAG).

711件の閲覧回数
kijimatomonori
Contributor I

I have a question about TAP reset of MPC 866 (JTAG).
* JTAG is set to ENABLE in Hard Reset Configuration Word for MPC 866.

(1) Does the software reset (TCK 5 times while keeping TMS kept HIGH) work?

(2) Do you need some procedure to execute soft reset?

(3) Please tell me the reason why PORST and TRST are connected together.

0 件の賞賛
返信
1 返信

603件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

1. No, this type of reset is not supported in MPC8xx family devices.

2. Please assert TRST input to do that.

3. TRST is typically connected to PORESET to assert TRST at power on simultaneously with PORESET.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信