How to flash u-boot to NOR flash(MT28EW128) using Codewarrior 8.8 (MPC8248)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to flash u-boot to NOR flash(MT28EW128) using Codewarrior 8.8 (MPC8248)

ソリューションへジャンプ
2,076件の閲覧回数
winstonjacob
Contributor IV

I am using MPC8248, and I need to bring up the board using NOR flash, so I need to flash the U-boot to NOR flash using Codewarrior 8.8, If anybody have the document, please share with me.

 

Regards,

Winston.

0 件の賞賛
返信
1 解決策
2,065件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

For flash programming in CodeWarrior 8.8, please refer to the attached ppt.

MT28EW128 is not provided in flash programing device list in CodeWarrior 8.8. 

The MT28EW is compatible with the S29GL-P and S29GL-N 128Mb, 256Mb, 512Mb, and 1Gb devices, please try to use  S29GL-P and S29GL-N device for programming your device.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,066件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

For flash programming in CodeWarrior 8.8, please refer to the attached ppt.

MT28EW128 is not provided in flash programing device list in CodeWarrior 8.8. 

The MT28EW is compatible with the S29GL-P and S29GL-N 128Mb, 256Mb, 512Mb, and 1Gb devices, please try to use  S29GL-P and S29GL-N device for programming your device.

0 件の賞賛
返信