How to Execute A-008109 erratum workaround

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Execute A-008109 erratum workaround

ソリューションへジャンプ
4,144件の閲覧回数
singhawadhesh
Contributor I

Hi Team,

I am working on T2081 based custom board. I have soldered discrete DDR3L (micron-MT41K512M16) on it.

I am unable to configure and initialize through the QCVS tool.

While debug  found a errata A-008109 (in T2080CE-Rev5.pdf) related to soldered discrete DDR3L as:

A-008109: Memory controller could fail initialization with soldered down register and
discrete DRAM

To apply this I need to update DEBUG_19 and DEBUG_29 as input.

Please could you let me know where/which file should I update to apply the changed value.

 

Thanks and warm regards,

Awadhesh Singh

0 件の賞賛
返信
1 解決策
4,112件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please provide the processor to SDRAM connection schematics as searchable PDF for inspection.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,139件の閲覧回数
ufedor
NXP Employee
NXP Employee

The erratum is not applicable if there is no soldered down register in the design.

0 件の賞賛
返信
4,129件の閲覧回数
singhawadhesh
Contributor I

Hi Fedor Bayev,

I have soldered down register and discrete DDR3L (micron-MT41K512M16) in my custom design.

Would the erratum applicable for this and how to execute this workaround?

Thanks,

Awadhesh 

0 件の賞賛
返信
4,113件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please provide the processor to SDRAM connection schematics as searchable PDF for inspection.

0 件の賞賛
返信