How are POWERQUICC processors affected by Sectre and Meltdown?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How are POWERQUICC processors affected by Sectre and Meltdown?

2,800 Views
mattfromseattle
Contributor I

For the recent Spectre and Meltdown security vulnerabilities, https://spectreattack.com/ , are the POWERQUICC family of processors vulnerable to either of these vulnerabilities?

4 Replies

1,965 Views
ToniZollikofer
NXP TechSupport
NXP TechSupport

Hello Matt,

NXP advises customers to write an email to the NXP Product Security Incident Response Team at psirt[@]nxp.com. It is required that you indicate the specific part and operating system that your question refers to in order to be able providing support in the best way.
For end users using NXP processors but not buying semiconductors from NXP directly or through distributors, we have to refer to the original equipment manufacturer (OEM) as any security analysis needs to be done on a system level.


Have a great day,

Toni
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,965 Views
alexander_yakov
NXP Employee
NXP Employee

Detailed investigations are running, we will come back with more information. Thanks for you patience.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,965 Views
SLICE
Contributor IV

Dear team,

My customer also is using P1010 and P2041, and they need to know if it affect also on PPC.

Thanks,

Miyamoto

0 Kudos
Reply

1,965 Views
matevzlangus
Contributor III

if it helps, we checked P4080 and T4240

0 Kudos
Reply