Firmware/Software inside MPC8533?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Firmware/Software inside MPC8533?

ソリューションへジャンプ
1,794件の閲覧回数
Rioss
Contributor I

I have read the documentations of MPC8533. But I am still not sure that MPC8533 can store firmware/software inside it? (for example: boot software). It is an integrated processor, not a traditional processor.

Can you help to confirm that it can store firmware/software inside it or not?

0 件の賞賛
返信
1 解決策
1,762件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

firmware/software cannot be stored in MPC8533 processor, it should be deployed on the boot media device integrated on the target board, for example eLBC NOR flash or SD card.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,763件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

firmware/software cannot be stored in MPC8533 processor, it should be deployed on the boot media device integrated on the target board, for example eLBC NOR flash or SD card.

0 件の賞賛
返信
1,749件の閲覧回数
Rioss
Contributor I
Thank you very much for your help.
0 件の賞賛
返信