Firmware/Software inside MPC8533?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Firmware/Software inside MPC8533?

Jump to solution
1,795 Views
Rioss
Contributor I

I have read the documentations of MPC8533. But I am still not sure that MPC8533 can store firmware/software inside it? (for example: boot software). It is an integrated processor, not a traditional processor.

Can you help to confirm that it can store firmware/software inside it or not?

0 Kudos
Reply
1 Solution
1,763 Views
yipingwang
NXP TechSupport
NXP TechSupport

firmware/software cannot be stored in MPC8533 processor, it should be deployed on the boot media device integrated on the target board, for example eLBC NOR flash or SD card.

View solution in original post

0 Kudos
Reply
2 Replies
1,764 Views
yipingwang
NXP TechSupport
NXP TechSupport

firmware/software cannot be stored in MPC8533 processor, it should be deployed on the boot media device integrated on the target board, for example eLBC NOR flash or SD card.

0 Kudos
Reply
1,750 Views
Rioss
Contributor I
Thank you very much for your help.
0 Kudos
Reply