DQS configuration for MPC8349EA (DQS_CFG field)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DQS configuration for MPC8349EA (DQS_CFG field)

ソリューションへジャンプ
938件の閲覧回数
mallik
Contributor II

Hi,

MPC8349EA has single ended strobe MDQS[0-8].

But the reference manual Table 13, Pg 385

says, DQS can be configured for Either Differential or single ended signal.

Whether we can configure DQS as Differential in MPC8349EA-667Mhz

ラベル(1)
  • DDR

タグ(1)
1 解決策
727件の閲覧回数
Bulat
NXP Employee
NXP Employee

It is a mistake in the manual that has been already fixed. Please take a look at the manual errata (MPC8349EARMAD), it states:

"9.4.1.8, 9-23 Changed setting 01 of DDR_SDRAM_CONFIG_2[DQS_CFG] to reserved."

So no, differential DQS is not available and can not be configured in the MPC8349.

元の投稿で解決策を見る

1 返信
728件の閲覧回数
Bulat
NXP Employee
NXP Employee

It is a mistake in the manual that has been already fixed. Please take a look at the manual errata (MPC8349EARMAD), it states:

"9.4.1.8, 9-23 Changed setting 01 of DDR_SDRAM_CONFIG_2[DQS_CFG] to reserved."

So no, differential DQS is not available and can not be configured in the MPC8349.