DDR DRAM mode register address bits

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR DRAM mode register address bits

Jump to solution
2,389 Views
dallasclow
Contributor II

Are the bank address bits of the mode register settings (two msb's) of each field in DDR_SDRAM_MODE and DDR_SDRAM_MODE_2 used by the DDR controller at initialization or are they ignored?  There is a separate field for each specific mode register, which should allow the bank address bits to be ignored when addressing the DRAMs.  We're trying to assess the impact of a SW bug that incorrectly set the two msb's of the ESDMODE, ESDMODE2, and ESDMODE3 fields.  Would these to bits be ignored or cause incorrect DRAM mode register writes?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,331 Views
ufedor
NXP Employee
NXP Employee

> Would these to bits be ignored or cause incorrect DRAM mode register writes?

These bits are ignored.

View solution in original post

3 Replies
2,331 Views
dallasclow
Contributor II

This is an MPC8610.

0 Kudos
Reply
2,332 Views
ufedor
NXP Employee
NXP Employee

> Would these to bits be ignored or cause incorrect DRAM mode register writes?

These bits are ignored.

2,331 Views
ufedor
NXP Employee
NXP Employee

Which processor is in question?

0 Kudos
Reply