Compilation guide of LTIB of MPC8308 in Ubuntu-14.04

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Compilation guide of LTIB of MPC8308 in Ubuntu-14.04

1,003 次查看
nthiru28
Contributor I

Hi All,

I'm trying to compile the BSP of MPC8308RDB LTIB (770-77823.iso) in ubuntu-14.04. There is no smooth way of completing the compilation.

Please suggest me the correct way of install and compilation of BSP in ubuntu-14.04 LTS

Regards,

Thiru N

0 项奖励
回复
1 回复

771 次查看
alexander_yakov
NXP Employee
NXP Employee

LTIB is quite old software and initially it was designed to run on redhat-type systems.

It is also possible to run LTIB on ealier versions of Ubuntu with just a minor additional packages installed.

But starting from Ubuntu 12.04, LTIB does not work on Ubuntu without special patch.

Please seach this community for "Ubuntu Ltib patch".

For example, please look the following link:

ubuntu-ltib-patch.tgz

0 项奖励
回复