Compatibility of MPC8306 interface with micron DDR2 SDRAM (vendor part no. MT47H128M16RT-25E)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compatibility of MPC8306 interface with micron DDR2 SDRAM (vendor part no. MT47H128M16RT-25E)

1,116件の閲覧回数
ankitasaldhi
Contributor I

We would like to interface two micron DDR2 SDRAM IC (vendor part no. MT47H128M16RT-25E) with MPC8306. Is this DDR2 IC compatible with MPC8306?

ラベル(1)
  • DDR

0 件の賞賛
返信
1 返信

802件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,
 

Yes MT47H128M16RT-25E looks compatible with MPC8306. The MT47H128M16RT supports 200MHz clock, however it will operate at 167 MHz which is maximum for the MPC8306 DDR controller.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信