CPU mpc8315e hangs if I touch its top surface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CPU mpc8315e hangs if I touch its top surface

ソリューションへジャンプ
1,436件の閲覧回数
zhenhuan
Contributor I

what  is possible reason?

0 件の賞賛
返信
1 解決策
1,354件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

The most probable reason - some input pin may be left unconnected and acts as antenna.

元の投稿で解決策を見る

3 返答(返信)
1,355件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

The most probable reason - some input pin may be left unconnected and acts as antenna.

1,354件の閲覧回数
zhenhuan
Contributor I

It turned out that  TEST_MODE pin (D6) was left unconnected, it shold be the reason.

0 件の賞賛
返信
1,354件の閲覧回数
LPP
NXP Employee
NXP Employee

Also, it migh be a failed joint under the package that bounces under the pressure. You can distinguish between two reasons by touching the package by a plastic stick rather than by a finger.

0 件の賞賛
返信